AnsweredAssumed Answered

AD9364

Question asked by hplee on Nov 7, 2016
Latest reply on Nov 8, 2016 by Vinod

Hi EZ support,

Customer managed to read the input from their customised board design but the performance is not desirable (bad performance) as compared to FMCOMMS2 board.

Input signal is a 2.405GHz signal at -30dbm.

The local oscillator frequency I set is at 2.4GHz.

Expecting to read out a signal of 5MHz.

 

See attached file (schematic and plot).

 

 

They would like to know how ADI recommends designing the traces for the input RF.

  • Impedance matching of the lines connected to the Balun. They are using the same Balun as FMCOMMS2 and is also taking in a Single-Ended input and converting it to differential.

o   Is the single ended input line to the Balun 50ohm impedance, while the differential output is 100ohm impedance?

  • Can I check if the Clock selection is ok?

o   Using (ASDM1-33.333MHZ-LC-T) together with a voltage level translator (SN74AUC1G125).

  • Can I check if the stability is good enough? The oscillator is rated at +/-50ppm.
  • Can I check if adding the voltage level translator will affect the performance?

 

 Please advise...

 

 

Thank you.

 

 

Regards,

HP

 

Attachments

Outcomes