AnsweredAssumed Answered

112409-HMC814LC3B low output power

Question asked by Vladimir.Matvejev on Nov 7, 2016
Latest reply on Dec 8, 2016 by dmailloux

Dear,

 

I obtain 112409-HMC814LC3B output power lower that specified.

 

I am using EV-ADF5355SD1Z frequency synthesizer to generate ~+2 dBm at 7.25-7.75 GHz signal (harmonics: -6dBm at 3.6-3.9GHz and -15dBm at 10.9-11.7 GHz). The signal is fed directly to active frequency doubler 112409-HMC814LC3B to get 14.5-15.5 GHz signal. According to the datasheet 112409-HMC814LC3B output power level should be >+15dBm, but I only measure 0 to +6dBm at the output. What could be a reason for such a low output power?

 

I use one lab power supply to supply +5V at 80mA both Vdd1 and Vdd2. I have tested two evaluation boards  112409-HMC814LC3B with the same result. I also use 115739-HMC573LC3B in the similar way and I get the right output power levels.

 

Thank you for your help.

 

Kind regards,

Vladimir

Outcomes