AnsweredAssumed Answered

ICE-1000 doesn't load the Programm to ASDP-21489

Question asked by WanneBe on Nov 7, 2016
Latest reply on Dec 7, 2016 by Kader.M

Hello together,

related to a study project I have to connect an ICE-1000 to a costum Board (ADSP-21489). But unfortunatly I can not get it running. Even when CCES says „Load complete“ and the LED switches from Green to Magenta it does not do anything. Also it is not possible to set Breakpoints „Breakpoint insertion failure at FIR_Hardware.c [line: 29].  [TpsdkServer] Failed to set breakpoint at file ... “.  Automatic Breakpints like „main“ are ignored.

According to the test in Debug Configurations-> Select Session-> Configurator->Test… everything works.

I am useing CrossCore Embedded Studio 2.3.0 on Windows 8.1

For testing I set up a very small programm wich is compiled without errors.

void main(void)

{

       int i;

       /* Initialize managed drivers and/or services */

       adi_initComponents();

 

       /* init PLL, do this before UART, etc. */

       Init_PLL();

       /*init SDRAM */

       Init_SDRAM();

 

             while (1) {

                    printf("hello\n");

                    }

}

 

Does someone has an idea what I could try to make this work?

Kind regards

Raphael

Outcomes