AnsweredAssumed Answered

ADAS1000  ECG Output

Question asked by BME>Mostafavi on Nov 4, 2016
Latest reply on Feb 1, 2017 by CatherineR

Hello

I using Adas1000 to capture LA ECG Channel.

My output is always zero & sometimes DRDY stays busy for very long time

first my code waiting for device initialize ,when DRDY goes 0 start to config

then the DRDY become to level sensitive for frame data ready


                      if (DRDY==0)
                        {   //do framing mode                              
                         }
                      else if(DRDY==1)
                        { // print  busy
                         )
                            
                     

my configures are below:

32 bit write commands
// FRMCTL config

0x8A7FFE00
// ECGCTL config    
0x81800022
// ECGCTL start conversions
0x81800026

//then start command

0x40000000

I using 2kh frame rate

internal clock source

frame content just LA word

2 word per frame

I can correctly communicate with device

write a register and read each of them

Like PACEAMPTH

when I read LA register 0x11

i receive zero

or at framing mode i always give zero on output.

what is wrong with my code or config?

 

Outcomes