AnsweredAssumed Answered

Is there a way to create a cyclic buffer in Matlab?

Question asked by ChrisB Employee on Oct 31, 2016
Latest reply on Oct 31, 2016 by ACozma

Hello all,

 

I'd like to use Matlab with FMCOMMS2/3/5. I can connect to the ZC706 and control the AD9361.

Ideally, I'd like to configure the TX part of the AD9361 to continuously (without gaps) play back a certain pattern. When the complete system is in a settled state, I'd like to trigger a capture and work on the RX received data.

I understand that IIO supports cyclic buffers. There is a special parameter when creating the buffer in C.

Would it be possible to create same cyclic buffer functionality in Matlab?

Or is Matlab always "streaming"?

Outcomes