AnsweredAssumed Answered

EVAL-AD7768-4 Software Issue

Question asked by Wade.Calcutt on Oct 31, 2016
Latest reply on May 17, 2017 by jcolao

I'm using the software application for the EVAL-AD7768-4 evaluation board. Whenever I attempt to change settings on the 'Configuration' tab in the software I get a condensed pop-up window (except when selecting the 'Precharge Buffers' option) that won't allow any changes to be made. In all cases upon closing the condensed window an error window pops up with the following info:

 

Error 1 occurred at Generate User Event in Pop-up Event Handler__adi.lvclass:Target 1.vi

Possible reason(s):

LabVIEW: An input parameter is invalid. For example if the input is a path, the path might contain a character not allowed by the OS such as ? or @.

 

While I can make configuration changes using the 'Registers' tab it would be much more convenient to use the 'Configuration' tab. Any ideas on how to fix this issue? Examples of condensed window and error window are attached.

 

The software is version 1.0 and was installed with all default settings.

Attachments

Outcomes