AnsweredAssumed Answered

No-OS Command line control of AD9361s in FMCOMMS5

Question asked by ThomasCook on Oct 28, 2016
Latest reply on Nov 1, 2016 by DragosB

Getting started with the ZC706 with FMCOMMS5 and no-OS software, I want to use the CLI commands to control frequency and phase of DDS outputs for all four RF channels (two AD9361s).  But I only see commands for controlling two channels (TX1,TX2,RX1,RX2) in the command line interface. 

 

In the code I see functions in ad9361_api.c that show support for all four channels, and it looks like both are both configured upon startup with default data structure settings.  But it does not appear to me that the CLI interface code in command.c provide control of the second AD9361 (channels 3,4) specific to the FMCOMMS5 board. Please advise.

Outcomes