AnsweredAssumed Answered

Powering AD5360 with only DVcc  

Question asked by SureshSurya on Oct 28, 2016
Latest reply on Nov 3, 2016 by Mike_OBrien

Hi,

I am using AD5360 in my design. The module contains various power supplies such as +3.3V (DVcc), +15V (VDD) and +-15V (VSS). +15V and -15V is used only this interface. Can I Power On the module with only +3.3V (without +15V and -15V) for testing other interfaces of the module?


Powering the AD5360 device with DVcc alone has any adverse effect??

 

Kindly advise.

 

Surya

Outcomes