AnsweredAssumed Answered

AD9371 Transceiver Evaluation Software and Filter Wizard issues

Question asked by A.P on Oct 26, 2016
Latest reply on Nov 21, 2017 by gverma

I have been working with the AD9371 evaluation board, and can connect and stream data with the oscilloscope application. I am however unable to use the Evaluation Software. When I put in the TCP IP Address of the board and hit connect, I get the error below:

What exactly needs to be done for this program to work?

 

Also, I was using the MATLAB Filter Wizard to generate the receiver FIR filters, which worked fine. However, the output of the filter wizard is a .txt file, and when trying to load it into the board with the Oscilloscope application, I get an error because it isn't a .ftr file. The conversion of the .txt file to the .ftr file is handled by the Evaluation Software before being loaded into the board, but since I cannot use the Evaluation Software, I also cannot use the Filter Wizard. What should I do to fix these issues?

 

Thank You

Outcomes