AnsweredAssumed Answered

change default speed of SPI Master boot for BF537

Question asked by MattZ on Oct 24, 2016
Latest reply on Oct 25, 2016 by MattZ

Hi All,

 

I understand that in SPI Master Boot Mode (BMODE = 011) the SPI baud rate register is set to 133 and therefore the default baud is SCK/(2 x 133). Is there a way to change that default "133"?

 

I suspect that way to do that is to set something in my Initialization Code somewhat analogous to how the documentation shows one can configure the SDRAM. Can anyone point me to sample code on how to set the baud rate in my Initialization Code?

 

Thanks in advance.

Outcomes