AnsweredAssumed Answered

Where is the Full-Range RMS Compressor?

Question asked by electrojim on Oct 24, 2016
Latest reply on Oct 29, 2016 by electrojim

I'm running Sigma Studio 3.13, Build 4 under Windows 10, and am in the menu tree for the ADAU1451.  Under Dynamics Processors / RMS / Full Range (-140dB to +40dB) / No Ext Detector Input / 1(or 2)-Channel/RMS (no gain), I open Show Graph and see a part that only goes from -135dB to +20dB, like the 'Lower Range' parts.  The corresponding Peak Limiter block goes all the way, but these don't.  What am I missing?

Attachments

Outcomes