AnsweredAssumed Answered

AD9361 with ZC702   1)When using the NO_OS API and in particular the adc_capture( ) routine what is the maximum number of samples on a single channel?

Question asked by numismaster on Oct 19, 2016
Latest reply on Oct 20, 2016 by DragosB

On the FMCOMMS2 evaluation board. We are using a ZC702 board..

 

Two things: 

 

  1. When using the NO_OS API and in particular the adc_capture( ) routine what is the maximum number of samples on a single channel?

 

      2) Can we operate receiver on the AD9361 channel 1 with a different BB filter bandwidth than channel 2 (18 MHz and 5 MHz, or 5MHz and 1.4 MHz) and perform simultaneous adc_captures( )?

Outcomes