AnsweredAssumed Answered

fmcomms5 reference hdl

Question asked by lesley on Oct 18, 2016
Latest reply on Oct 25, 2016 by rejeesh

Hi all,

   I have several questions of the ADI reference hdl design of FMCOMMS5 +ZC706:

   1、Why do you connect the "clk" pin of axi_ad9361_1 to the "l_clk" of axi_ad9361_0 in the design?

   2、Are "clk" of axi_9361_0 and axi_ad9361_1 used for FPGA as data transmission clock?

        If yes, why the clocks in i_tx_data and i_tx_frame module are still "l_clk" (generated from the respective data_clk transmitted from ad9361)? And why the clocks of i_rx (axi_ad9361_rx) and i_tx (axi_ad9361_tx) modules are "clk"?

 

         

//////

///////

          

   

   3、Based on the questions above, I am wondering what's the differences and relationship between i_tx_data(i_rx_data), i_tx_frame(i_rx_frame) and i_tx(i_rx)?

FPGA Reference Designs

Design Support AD9361/AD9363/AD9364

stevebkaushalJohannesH

Outcomes