AnsweredAssumed Answered

AD9467-FMC-250EBZ reference design

Question asked by nerdler33 on Oct 14, 2016
Latest reply on Oct 17, 2016 by CsomI

Hello,

I am in the process of building the AD9467-FMC-250EBZ reference design. Using vivado 2016.2, when I try to use the tcl file to build the project, I get the following error: 

ERROR: [BD 41-1075] Cannot create address segment for </axi_hdmi_dma/S_AXI_LITE/Reg> in </sys_ps7/Data> at 0x43000000 [ 256 ]. Range = 256. Memory ranges must be at least 4K.
ERROR: [BD 5-14] Error: running create_bd_segment.
ERROR: [Common 17-39] 'create_bd_addr_seg' failed due to earlier errors.

while executing
"create_bd_addr_seg -range $p_seg_range -offset $p_address $sys_addr_cntrl_space $p_seg_name "SEG_data_${p_name}""
invoked from within
"if {$p_index == 0} {
set p_seg_range [get_property range $p_seg_name]
create_bd_addr_seg -range $p_seg_range -offset $p_address $sys_addr..."
("foreach" body line 2)
invoked from within
"foreach p_seg_name $p_seg {
if {$p_index == 0} {
set p_seg_range [get_property range $p_seg_name]
create_bd_addr_seg -range $p_seg_ran..."
(procedure "ad_cpu_interconnect" line 69)
invoked from within
"ad_cpu_interconnect 0x43000000 axi_hdmi_dma"
(file "../../../projects/common/zed/zed_system_bd.tcl" line 271)

while executing
"source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl"
(file "system_bd.tcl" line 2)

while executing
"source system_bd.tcl"
(procedure "adi_project_create" line 97)
invoked from within
"adi_project_create ad9467_fmc_zed"

 

I have not done anything except for build the libraries required and ran the tcl file in the reference project. 

Any help understanding this error would be greatly appreciated. 

 

Thank you,

Tyler

Outcomes