AnsweredAssumed Answered

(ADV7181D)Which format does ADV7181D supports.

Question asked by donadona999s on Oct 14, 2016
Latest reply on Oct 17, 2016 by donadona999s

Hi!

 

I have a question about ADV7181D.

Maybe I should not ask about this to you but I would be glad if you can help me.

 

The input resolution is 480i with CVBS.

Our customer are thinking to use two ADV7181D .

One will output 8Bits 27MHz.

One will output 16Bits 13.5MHz.

 

Q1)

I think 8Bits output is based on BT.656.

Is this correct?

 

Q2)

Which video format will be use when our customer output 16Bits 13.5MHz.

Would it be BT.601?

 

Sorry...

I'm not sure what is BT.656 or BT.601 or BT.xxx ...

So if you can answer about this , it would help us very much.

 

Best regards.

Kawa

Outcomes