AnsweredAssumed Answered

Source code for the ADRF6806 GUI setup program

Question asked by Indra on Oct 13, 2016
Latest reply on Dec 1, 2016 by jdobler

Hi,

 

I am evaluating a new design using two ADRF 6806 boards simultaneously.

 

 

I need to be able to programmatically setup the two ADRFs which will then become part of a bigger program. The settings will only need to be setup at power up as the ADRFs will function at the setup frequency as long as the device is powered up.

 

Is it possible to get the source code for the ADRF6806 GUI program so that I do not have to start from scratch the whole coding process ?

 

Thank you,

 

Indrajit.

Outcomes