AnsweredAssumed Answered

Debug vs Release mode

Question asked by Jerca on Oct 11, 2016
Latest reply on Oct 21, 2016 by Jithul_Janardhanan

Hi,

 

I`m testing the example project 21489 AD1939 C Sampled-Based Talkthru 48 or 96 kHz (Analog Devices\VisualDSP 5.0\214xx\Examples\ADSP-21489 EZ-Board) on the EVAL-AD1938AZ evaluation board (DACs as master, TDM, BCLK = 8.192 MHz, LRCLK = 32kHz, sample rate 32 kHz). I`m using the option to test the DACs only with some generated pure tones (uncomment //#define GENERATE_DAC_PURE_TONES_TEST in SPORT1_ISR_process_sample_.asm). The problem is that in Debug mode everything is fine, but in Release mode it`s not working. Any advice?   

Outcomes