AnsweredAssumed Answered

Need File System Service Clarification

Question asked by TRON on Aug 19, 2011
Latest reply on Aug 22, 2011 by MartinK

In the VisualDSP 5.0 Update 9, 9.1 Release Notes it is stated that

 

In the updated FSS, the FSD can query the PID for the max transfer size (bytes) with the
command,
{ ADI_PID_CMD_GET_MAX_TFRCOUNT, (void*)&MaxtransferSize },

 

But in the header file adi_fss.h it is stated as:

 

ADI_PID_CMD_GET_MAX_TFRCOUNT,           /* (0x000B8015) Get max number sectors for single transfer  */

 

am I right to assume the Release Notes are correct and the headerfile line comment is wrong as it should instead state Get max number of bytes for a single transfer ?

 

 

Also, I have noticed in the adi_fss.h header file that the Return Codes enum is missing an item of value 0x000B000F, so all items after ADI_FSS_RESULT_NOT_SUPPORTED are one-off of what their stated value is in the comments, making it confusing to debug the FSS's return codes.

Outcomes