memsuser

ADXL362 - Wake-up and autosleep

Discussion created by memsuser on Oct 7, 2016

Hi,

I would like the ADXL362 to be in wake-up mode while there is no activity, and transition in and out of full-bandwidth measurement mode based on activity/inactivity detection. For this, I set both the WAKE-UP and the AUTOSLEEP bits in register 0x2D to '1'. However, what I observe is that the device is always sampling at the low 6Hz rate, even after the STATUS register is showing activity detection.

I expected the device to transition to full bandwidth measurement mode as soon as activity is detected. 

 

What am I doing wrong?

 

Thank you

Outcomes