AnsweredAssumed Answered

EasyStack on SP601

Question asked by sulemanzp on Oct 4, 2016
Latest reply on Nov 1, 2016 by TonyM

Hi,

I have HMCAD1520 board and I want to evaluate on SP601 board. I downloaded Easysuite and installed it.

Then I followed "easystack_xilinxsp601_userguide.pdf" document but I am unable to found "EasyStack.mcs" in the installation folder.

But I found "hmc1520_sp601_rev118.mcs" file in that folder. So I assume that this may be newer version of EasStack.mcs file. So I followed the rest of the steps and finally the LED on board start blinking. The issue is GPIO_LED0 is off which is opposite to this statement of the document "GPIO_LED0 should then be constantly lit". Also Easy_Suite shows couple of errors, I attached error pics in the end of the question.

My SP601 board Status after programming BPI Flash with the "hmc1520_sp601_rev118.mcs" file:

GPIO_LED0 = OFF

GPIO_LED1 = BLINKING

GPIO_LED2 = ON

GPIO_LED3 = ON

 

So if there is any other MCS file please let me know where from I can get it to test HMCAD1520 on SP601.

Attachments

Outcomes