AnsweredAssumed Answered

ADV7181C Evaluation Board MC/PC Switch

Question asked by jmdejoanelli on Oct 3, 2016
Latest reply on Oct 3, 2016 by JeyasudhaMuthuPerumal

Hi,

 

I have purchased an ADV7181C evaluation board (EVAL-ADV7181CEBZ).

I am trying to configure the registers of the board via "ADV Register Control 7.0", but when I select the available script via Setting -> Scripts -> CP XGA 1024x768 -> RGB 1024x768@60Hz 12-Bit DDR 65.000MHz out through HDMI.

 

A message box then pops up displaying "Switch MC/PC Switch to PC and Reset All Boards". See attached image. When I click OK, I then see a message saying "Device 74: USB Error (19)" along with multiple I2C errors.

  

The user manual for the software doesn't seem to offer any help with this particular problem. Can you provide some guidance?

 

Also, under the options menu and in the manual, there is reference to a CSC Mapping Utility program. Where can I access this software?

 

Regards,

Josef

Attachments

Outcomes