AnsweredAssumed Answered

AD9652 ADC tSKEW Min/Max Switching Specifications

Question asked by Freddy_Y on Sep 30, 2016
Latest reply on Oct 11, 2016 by Freddy_Y

Hi,

    AD9652 ADC switching specifications are:

DCO±-to-Data Skew (tSKEW) Typical 0 ns

(see datasheet Rev. A on page 7)

 

Which is the min and max value?

I've to interface this ADC device with device with an FPGA at 307.2 MHz clock rate so I need the min/max tSKEW in order to make sure the interface timing are proper.

Thanks.

Outcomes