AnsweredAssumed Answered

HMC6300/HMC6301

Question asked by Jeoy on Sep 30, 2016
Latest reply on Jan 5, 2017 by Mark_D

Hello, I plan to purchase The EK1HMC6350 evaluation kit. According to the information on your company’s website,There are two motherboards in the kit: an HMC6300 motherboard with the TX module location populated and the HMC6301 motherboard with the RX module location populated.” That is to say, HMC6300 motherboard is just equipped with TX module and HMC6301 motherboard is just equipped with RX module. Based on these information, there are several questions I want to seek your answers.

Except the RX module location and the TX module location ,are these two motherboards the same If not, can we assemble one motherboard with the RX module location and the TX module location at the same time? Will it work?

 Evaluation software CD-ROM contains the HMC6300/HMC6301 Graphical User Interface software GUI. Can these two software program the HMC6300 and HMC6301 on the same motherboard by writing to the device registers at the same time? Will it conflict?

I really hope someone can answer my questions timely.

That’s all. Thank you.

Outcomes