AnsweredAssumed Answered

I am using the AD7476 1 MSPS serial ADC.  The fclk frequency is 12 MHz. I see 4 short 20 ns pulses on the SDATA line from the ADC framed by the chip select line, /CS.  The short SDATA pulses are always 4 clock pulses apart, 320 ns.  If anyone can explain

Question asked by kaquino on Sep 28, 2016
Latest reply on Sep 29, 2016 by jcolao

I am using the AD7476 1 MSPS serial ADC. The fclk frequency is 12 MHz. I see 4 short 20 ns pulses on the SDATA line from the ADC framed by the chip select line, /CS. The short SDATA pulses are always 4 clock pulses apart, 320 ns. If anyone can explain this I would very much appreciate this.

Outcomes