AnsweredAssumed Answered

IBIS model parameter

Question asked by donadona999s on Sep 28, 2016
Latest reply on Sep 29, 2016 by donadona999s

Hi !


I have a question about IBIS model parameter.

For example ADV7511W's IBIS model is this .

 

There is no parameter for 1~15pins at this picture.

 

1)

Does this mean the parameter is contained to the Package parameter?

 

2)

For example , 16Pins(HPD) has the PLC parameter for this pin.

Does this means , when the customer simulate the IBIS model, simulator will add the pin parameter and package parameter?

 

3)

Is this parameter made from simulation only?

Or do ADI measure the device?

 Our customer want to know how ADI made this IBIS model.

 

Best regards,

Kawa

Outcomes