AnsweredAssumed Answered

Bare metal examples for BF527

Question asked by augie on Aug 17, 2011
Latest reply on Aug 29, 2011 by CraigG

I'm trying to find any bare metal examples for the BF527. Specifically for the SDP-B if possible. Like the proper linker definitions; C SDK/API information. I can download and run a small app using the GNU toolchain and a JTAG interface. I want to know how to create an image that will flash and run standalone. Also if there are any C-level libraries I can use to communicate with resources like USB and SPORT so I don't have to figure out all the registers. If I have to that's fine...I just don't want to re-invent the wheel if these things exist. So far I don't see anything like this that doesn't run under uCLinux or some OS. Is that really the case?

Outcomes