AnsweredAssumed Answered

MOG with goVosConfig.outputDiffVal = 1

Question asked by chiara.bizzotto on Sep 20, 2016
Latest reply on Oct 7, 2016 by chiara.bizzotto

I want to see the output of the VOS process with the goVosConfig.outputDiffVal set to 1, that is before any morphology happens. For the File IO demo do I have to modify/add something else? Because when I try it crashes after processing one frame.

 

A non-recoverable error or exception has occurred.
Description: A data CPLB miss has occurred without a corresponding CPLB entry.
General Type: RunTimeError
Specific Type: DCPLBMissWithoutReplacement
Error PC: 0x11a006ea

I don't know why CCES shows as if ENABLE_MOG_BINARY_OUT is not defined, but it is defined and the program goes into MogBinaryImageOut().

 

 

 

Am I missing something?

Everything works fine with goVosConfig.outputDiffVal set to 2.

 

Thanks in advance! 

Outcomes