AnsweredAssumed Answered

Will a AD-FMCOMMS3-EBZ like design work without a FRU EEPROM

Question asked by dmitriy00 on Sep 20, 2016
Latest reply on Sep 22, 2016 by larsc
Branched from an earlier discussion

Hi Robin,

 

We plan to connect our own RF design containing the 9361 to ZC702 platform through the FMC connector. We don't have the I2C EEPROM and ADC to measure the power rails. Other than that the connections are identical to the FMCOMMS3 board. We only plan to use the IIO Scope to evaluate the RF circuit. I'm afraid now that ZC702 platform won't even see our board. Do I have a valid concern? If yes, is there a workaround to allow your software to still talk to and get the signals to/from the AD9361? Thanks.   

Outcomes