AnsweredAssumed Answered

ADG5404 Current

Question asked by andytian on Sep 18, 2016
Latest reply on Sep 19, 2016 by andytian

Hi, 

   I am using ADG5404F as Multiplexer, but encounters several questions. 

  1) In my application, 100~200mA continuous current is needed, is ADG5404F ok?

  2) I check the datasheet, it mentions continuous current up to 280mA(Table 5), but in ABSOLUTE MAXIMUM RATINGS, 'D pin to GND' is limited to 'VSS-0.7V to VDD+0.7V or 30mA, whichever occurs first'. then, I am confused, which one should i adopt?

   Thank you much.

Attachments

Outcomes