AnsweredAssumed Answered

How to set up AD9164 to operate in 2x NRZ mode?

Question asked by blue_angel on Sep 16, 2016
Latest reply on Dec 21, 2016 by danf

I would to use AD9164 in the 2xNRZ mode in order to generate a signal in 0 - 3 GHz BW.

ad9164 ads7-v2ebz

I'm using  ADS7-v2 board and AD9164-FMC-EBZ mezzanine.

 

Is possible to set up the DAC in order to generate a 3 GHz single tone without his spectral component mixed with the Fc/2 frequency?

 

Thanks in advance.

Kind regards

Federico

Outcomes