AnsweredAssumed Answered

Level detect readout via I2C (ADAU1702)

Question asked by mantabernd on Sep 15, 2016
Latest reply on Jan 12, 2017 by andrei_eugen

Hello,

 

I actually try to read out a level detect block from SigmaStudio via I2C.

 

in my .params file I can see following block:

 

Cell Name = 1 X RTA1
Parameter Name = SingleBandLevelDet1decay
Parameter Address = 45
Parameter Value = 0.000108480453491211
Parameter Data :
0x00 , 0x00 , 0x03 , 0x8E ,

 

If I readout 0x45, I get 0x00, 0x00, 0x03, 0x8E as result. But this value is never changing.

 

So which register should I readout to get the actual value of the level detect block?

 

Thanks in advance

Best regards

Bernhard 

Outcomes