AnsweredAssumed Answered

[BD 5-216] error in [building the project in Vivado2014.4]

Question asked by LI1234 on Sep 14, 2016
Latest reply on Sep 22, 2016 by LI1234
Branched to a new discussion

i'm using Zedboard + fmcomms2 and Vivado 2014.4, ISE 14.7(win32)

 

I download the hdl_2014_r1 in the GitHub - analogdevicesinc/hdl at hdl_2014_r1 and met an error  following the instruction of Building HDL [Analog Devices Wiki]

 

the error message is :

 

ERROR: [BD 5-216] VLNV <xilinx.com:ip:processing_system7:5.3> is not supported for this version of the tools.The latest version is:5.5

ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

 

 

    while executing

"create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.3 sys_ps7"

    invoked from within

"set sys_ps7  [create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.3 sys_ps7]"

    (file "../../../projects/common/zed/zed_system_bd.tcl" line 46)

 

 

    while executing

"source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl"

    (file "system_bd.tcl" line 2)

 

 

    while executing

"source system_bd.tcl"

    (procedure "adi_project_create" line 94)

    invoked from within

"adi_project_create fmcomms2_zc702"

    (file "./system_project.tcl" line 7)

what should I do more to process it completely?

Outcomes