AnsweredAssumed Answered

USB Webcam Support for Analog Devices' Linux

Question asked by zacharyr on Sep 13, 2016
Latest reply on Sep 13, 2016 by zacharyr

Hello,

 

I have installed the 2015_R2 Linux image from the Analog devices wiki (Zynq & Altera SoC Quick Start Guide [Analog Devices Wiki]) and when I plug in my USB webcam (Logitech C920) there is nothing returned with the command ls /dev/video*. When I open VLC Media Player and go to Open Capture Device, there are no webcams listed under Video device name (usually says /dev/video0).

 

Is there no native USB webcam support in the 2015_R2 image? If there isn't, how can I recompile the 2015_R2 image with USB webcam support enabled?

 

If it helps, the device I am using is the ZC706.

 

Thanks

Outcomes