AnsweredAssumed Answered

AD9984A temperature range

Question asked by ysuzuki on Sep 12, 2016
Latest reply on Sep 12, 2016 by JeyasudhaMuthuPerumal

Hello support,

 

In the datasheet of AD9984A, there are two temperature range.

On the margin of page-3, temp. condition is indicated as "full temperature range = 0°C to 70°C." .

And in the page-5, operating temperature range is indicated as "-25°C to 85°C." .

 

Could you teach me the defference between "full temperature range" and "operating temperature range" ?

 

Best regards,

ysuzuki

Outcomes