AnsweredAssumed Answered

AD9361 Rx Specifications from 70 MHz to 6 GHz

Question asked by Ter on Sep 12, 2016
Latest reply on Sep 12, 2016 by Vinod

The AD9361 has detailed RX specifications at 900 MHz, 2.4 GHz, and 5.5 GHz.  Are there any additional graphs or data that covers the frequencies between these ranges. For instance what is the NF, max gain, IP3, and IP2 values from 70 MHz to 6 GHz?

Outcomes