AnsweredAssumed Answered

Is there a way to enter variables using stdin through the Console tab instead of the Input box, for instance how IAR allows it with their Eclipse plug-in?

Question asked by oldfoxsoftware on Sep 9, 2016
Latest reply on Sep 23, 2016 by NormY

I created a test menu using printf / stdout to the Console tab. I use scanf / getchar through stdin to get the user's menu choice. CrossCore Embedded Studio pops up an input box when these input functions are called. This is all great and very helpful, except that this input box is a modal window which prevents any other interaction with the IDE, for example setting a break point or scrolling the Console. Is there a way to configure the IDE so the input is managed through the Console or a modeless input box?

 

BTW, I use doctest for my tests.

Attachments

Outcomes