AnsweredAssumed Answered

(ADV7281-M)Start up time

Question asked by donadona999s on Sep 8, 2016
Latest reply on Sep 20, 2016 by donadona999s

Hi !

 

I have a question about ADV7281-M.

Our customer want to use ADV7281-M for the rear view camera for automotive.

It is very important to clear the KT-Law.

* KT-Law = Kids and Transportation Safety Act Law

So they have to output the image from the system very fast.

Our customer want to know how long would it take to ADV7281-M outputs the image.

From the power on , I think it would take for

  I2C access = maybe less than 100ms

  Analog input lock = 500~700ms

  Mipi block On and output = maybe less than 100ms

so maybe it would take less than 500ms~1s to start up the ADV7281-M.

 

Can you tell me how long would it take to output image data from ADV7281-M mipi port from power supply on?

It is OK that the value is no specification.

We can tell to the customer that the value is just for advice only.

 

Also this is the first time to support ADV7281-M so we just bought the ADV7281-M Eval board 

but it is shipping to my LAB.

It would take more few weeks so I cannot see this at the Eval board now.

 

Best regards.

Kawa

Outcomes