AnsweredAssumed Answered

rx sampling frequency and Logic analyzer in FMCOMMS5

Question asked by arm2 on Sep 7, 2016
Latest reply on Sep 14, 2016 by rejeesh

I am working on FMCOMMS5 with zc706 carrier board. When I set rx sampling frequency to any frequency more than 6 MHz and the click on "run trigger immediate" button in vivado logic analyzer, a new batch of  data is captured and shown in wave scope and every thing is fine. But for any sampling frequency less than 6 MHz(e.g. 5 MHz), the logic analyzer does not work. In other words, by clicking on "run trigger immediate", there is no update in wave scope and no data is captured. Please guide me to solve this problem because I want to work in 2.084 MHz. Note  that, I use "ad9361_set_rx_sampling_freq" function to set rx sampling frequency.  

Outcomes