AnsweredAssumed Answered

need help getting device to accept input

Question asked by Ant223 on Sep 2, 2016
Latest reply on Sep 6, 2016 by Ant223

hello, i'm pretty new to this and i've been having problems with the development kit. i've modified the blinky code to light the LED's when i ever i apply an input to a specific pin. the pin is ion the breakout board as is the 3.3 V i'm using. i'm using the breakout board with LK1 in position A and using J4 pin 40 for power and J2 pin 10 as the variable, however it doesn't seem to be working. any help would be appreciated as i'm just getting started and am a bit lost

Attachments

Outcomes