AnsweredAssumed Answered

single ended to differential conversion

Question asked by nisu.99 on Sep 2, 2016
Latest reply on Sep 7, 2016 by nisu.99

If my input analog signal is of 175 mV (or 0.175V) with respect to ground and i want to convert it to the differential signal than is it possible to convert it  by using AD8138?.  my required frequency is between 30Hz to 500Hz and at output side the differential voltage must be same 175mV.

Outcomes