AnsweredAssumed Answered

Band selection in ADF4360-7

Question asked by scopeman on Aug 29, 2016
Latest reply on Sep 1, 2016 by Brigid.Duggan

In my application, I need the band selected by the ADF4360-7 to be consistent.  Right now I see many boards where the loop is bi-stable - one with a control voltage of 1.2V and the other with a control voltage of 2.5V as I reprogram the device to the same frequency.  Seems as if there are 2 possible bands that could be picked.  My question is can the band be predictable by choosing the correct components/tolerances over all environmental conditions (0-55 C)?

Outcomes