AnsweredAssumed Answered

HMC547A

Question asked by ADIguy on Aug 26, 2016
Latest reply on Aug 31, 2016 by s.ilke

Hello,

 

Could you please tell me if the HMC547 can be used as follows:

 

Can the RF signal be passed through from the RF1 to RF2 pins and the RFC pin left open?

The control inputs would then be tied together and both driven to the same logic states. The intended operation is that in one state, the input is shunted to ground via the internal 50 ohm termination, and in the opposite state the signal is passed through the device.

 

Thanks.

Outcomes