AnsweredAssumed Answered

Matching between AD9516 and CLK buffer

Question asked by jhshin on Aug 26, 2016
Latest reply on Aug 30, 2016 by JLKeip

Hi,

My customer is using AD9516 with the clock buffer of TI as shown below(refer to attached datasheet).

She said that if 10MHz input of clock buffer was connected directly to REFIN of AD9516, there was no problem and when she checked clock performance on output of clock buffer, there was no problem also.

But she had  a problem that when REFIN of AD9516 was connected via the clock buffer, phase noise of AD9516 ouput was degraded.

Please advice the causes and solutions to the problem.

Thanks in advance.

Attachments

Outcomes