AnsweredAssumed Answered

Floating point values processing using the FMCOMMS5 board

Question asked by foukalas@gmail.com on Aug 24, 2016
Latest reply on Sep 5, 2016 by mhennerich

Hi,

This is about our LTE baseband implementation using the Zynq and FMCOMSS5 boards from Xilinx and AD respectively.

 

We have done all LTE baseband implementation in C code including frequency and frame offset correction similar to your Matlab LTE example found at GitHub. Our implementation is tested on a host PC that gives a zero BER confirm that the implementation is correct.

 

We run now the LTE baseband on the Zynq board using the AD-FMCOMSS5 board too. Our C implementation is provided in a 32-bit floating-point format. Thus, we get the discrete-time signal provided by the OFDM from our LTE Tx side baseband. The values of the discrete time signals are in 32-bit floating-point format and in order to send those values over the RF board (ad9361), we have to convert them into a 12-bit fixed-point format.

 

We have noticed that the smaller and the biggest values of our signal are between -3.5... and 3.4. Thereby, we choose a fixed-point representation of 9 binary digits (i.e. yyy.xxxxxxxxx), where we can represent numbers between -4 and 4. Finally, we add 4 zero bits at the end of the 12bit number making a 16-bit number to send. This is compatible to the format being processed by the AD-FMCOMMS5 boards as far as we know. 

 

From the Rx side now, we get the 16-bit number from the RF and discard the 4 most significant bits. Using the rest 12-bits, we do the dual actions; we convert the 12-bit numbers into a floating-point numbers and deliver them to our LTE Rx side baseband.

 

However, this implementation gives a calculated BER equal to 0.5. We are wondering what is going wrong, since all baseband components are correct including the frequency and frame-offset correction as well.

 

We cannot find an answer and we are asking your advice to this issue about the way of processing the floating-point values into the FMCOMSS5 board.

 

Regards,

Fotis

Outcomes