AnsweredAssumed Answered

AD9652 LVDS SYNC input

Question asked by massronchi on Aug 24, 2016
Latest reply on Aug 25, 2016 by PMH

Hi, I need to synchronize four AD9652 devices using the SYNC input, the setup and hold time for SYNC input is very stringent and LVCMOS fanout buffer are not suitable for synchronize four device. I notice that the SYNC input is an CMOS/LVDS and in the EVM schematic the input is 50Ohm AC terminated input that seams designed to handle an single-end LVDS output. Is that true ?
Thank you
Maxx

Outcomes