AnsweredAssumed Answered

ADuC7060 run in debug-mode but dosen't start indipendent

Question asked by Engeneer on Aug 24, 2016
Latest reply on Aug 25, 2016 by Engeneer

The Programm run in debug-mode also indipendent when debugging is stopped.

After a re-start caused of a power supply interrupt the ADuC7060 dosen't run in program. The Start-up-file ADuC706x.s is integrated.

The evaluationboard starts self-sufficient with the same program.

 

Is there something different between the ADuC7060 on the evaluationboard and without?

What can be the problem after re-start?

 

Many thanks in advance!

Outcomes