AnsweredAssumed Answered

ADG918 Suitable as a switch to select between two radios that tx/rx to a single antenna?

Question asked by roostdyk on Aug 21, 2016
Latest reply on Sep 2, 2016 by ndhull

As long as the transmit power of the radio modules is not too high, is the ADG918 suitable for switching two different radio modules (one 915MHz and one 2.4GHz) to use the same antenna connected to RFCOM? The ADG918 would need to be capable of allowing the signal received by the antenna to be routed to the selected module, and the selected module to transmit through the switch to RFCOM

Outcomes