AnsweredAssumed Answered

AES-PZSDRCC-FMC-G(hdl_2016_r1) build warning and run error.

Question asked by anguo on Aug 19, 2016
Latest reply on Oct 16, 2016 by anguo

Dear Community!

 

Hardware: picozed-sdr som(rev.c) + AES-PZSDRCC-FMC-G(rev.c);

Vivado : 2015.4.2;

HDL version: hdl_2016_r1(download at 2016.08.05);

Project: \projects\pzsdr\ccfmc; 

Reference documents: 

   1. ADI Reference Designs HDL User Guide [Analog Devices Wiki] 

   2. AD6676EVB [Analog Devices Wiki] 

   3. Building HDL [Analog Devices Wiki] 

 

I want to build a reference project for the hardware manually on Vivado(never used makefile), some warnings occurred when build the libraries and project. and sdk project run error when initialize AD9361.

 

1st: about the constrain file.

       VADJ SELECTION (P8) on the AES-PZSDRCC-FMC-G carrier board is open, means 1.8V for bank_12 and bank_13, but IOs of these banks is constrained to LVCMOS25 such as W15 , V19 ... in pzsdr_system_constr.xdc and system_constr.xdc. I cannot understand. 

 

2nd: warnings of Vivado project.

      more warnings occurred when building  libraries and project than that referenced in Building HDL. some ports have no connection and some parameters are not used. can i ignore these warnings? 

 

3rd: run error in sdk project.

     I downloaded a no-os-2016-R1.zip at 2016.07.27. and i used the files in /ad9361/sw in sdk project. I used CONSOLE_COMMANDS, XILINX_PLATFORM, PICOZED_SDR in config.h. the project printed "AD9361 initialization error" as the pictures. But the project can run ok if i program fpga with the bit file in sd card. 

 

Thinks!!! 

Outcomes