AnsweredAssumed Answered

Inquiry about the wavelength of product ADN3010-11

Question asked by Ting_ting on Aug 18, 2016
Latest reply on Nov 12, 2017 by Pinenuts

Dear technical staff,
I would like to inquire about the product ADN3010-11. Recently, I am looking for a high sensitivity optical receiver with a free space optical input window and bandwidth≥10GHz. And I found the product ADN3010-11 is a suitable option. However, the datasheet indicates that this product is “characterized only at original band (O band) wavelengths” since it has an antireflective coating (ARC) centered at 1310 nm. I would like to ask, does it possible if the product could be redesigned and characterized to 1550nm band, which is required in our current experiment? Thanks:)
Kind regards,
Tingting

Outcomes