AnsweredAssumed Answered

AD5791 Sampling rate

Question asked by YZhao on Aug 17, 2016
Latest reply on Jun 20, 2017 by Johannes2

Hi, I want to generate a single 1MHz sine wave or a dual 1MHz+300kHz wave from FPGA and send to AD5791 for analogue output.

 

1. Can the AD5791 generate signal up to 1MHz? 

2. Is the 35 MHz SPI clock equivalent to the sampling rate?

3. Is the 1 uS settling time for settling to all 20-bit or only 1-bit?

 

Thank you.

Outcomes